Hello,
My customer would like to confirm if there is any sequence requirement between VCC and VM like order from VCC to VM, slew rate of those or something like those. I understand there is no requirement since the datasheet says nothing about it except "The DRV8835 allows separation of the motor voltage and logic voltage if desired. If VM and VCC are less than 7 V, the two voltages can be connected", but would you please tell me about it?
Best Regards,
Yoshikazu Kawasaki