Can we control motor speed using this IC.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shubham,
Yes, you can control the speed by PWM'ing the inputs.
Hi Rick,
Thankyou so much for support, please comment on below query.
How do I calculated the frequency and pulse width as per the required speed?
Hi Shubham,
A starting point is to PWM @ 20 to 50kHz at the input. PWM between drive and brake mode
The duty cycle will set the speed. Assuming VM is set to the rated motor voltage, a rough calculation is desired_speed/full_speed of the motor.
Hi Rick,
Thanyou for the information.
One more query is which will be most preferrable way to control using PWM i.e. IN/IN mode or PH/EN mode?
Thankyou in advance