Other Parts Discussed in Thread: DRV2603, DRV2603EVM-CT
Hi Guys
Our customer wants to use our DRV2605, there are a few of questions below:
1. The motor used by the customer is a dual axis instead of a single axis. Can we support the vibration effect of the double resonant frequency(160Hz and 320Hz)? Mainly use 160Hz. Is it possible to adjust the resonance frequency to 160 Hz by calibration; How to perform this type of calibration?
2. Can our 123 vibration effects be customized? I mean we want to produce a variety of different effects If so, is there any relevant documentation explaining our special effects?
3. If we use DRV2603, can we provide customers with a DRV2603-based program or firmware to generate PWM vibration waveforms?
4. In addition to the handheld device application, is there an application for our product in the gamepad? What brand of handle?
Thanks. Your feedback are very appreciated.
-Pengfei