Hi,
since yesterday I have the Issue, that program downloading obviously is too fast and "Start Motor" button stays grey;
DRV8353Rx 1.0.1
DRV8353RSH EVM GUI slvc737a
What went wrong with my system?
Tahnks
Ludwig
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
since yesterday I have the Issue, that program downloading obviously is too fast and "Start Motor" button stays grey;
DRV8353Rx 1.0.1
DRV8353RSH EVM GUI slvc737a
What went wrong with my system?
Tahnks
Ludwig
Hi Adam,
The connections are physically okay.
In the device manager the TI debugger apperars without issues.
I tried two different powersupplies.
I completely reinstalled the GUI, as well.
I also replaced the DRV8353RS IC twice.
What else can it be?
Luke,
Can you try using CCS? This method the system can tell you if the connection to the MCU is working and the programming is succeeding.
You can also try to exchange the EVM for a new one through the TI estore.
Regards,
-Adam