Other Parts Discussed in Thread: DRV8353R
Dear Sirs,
Regarding DRV8353RH-EVM- I have little confusion about the maximum voltage that this Evaluation Module can safely carry.
The Gate Driver in the list is rated 102 V, in the description is 100 V and the maximum voltage for the EVM is 95 V.
Can this EVM safely work with 100.8 V (24S Li-ion battery pack ) or do I need another driver suitable for this voltage?
Can you recommend one.
Best Regards
Miroslav Malev