Hi Sir
My name is Jim, I am also working on BLDC motor controller project like the others. My supply voltage is about 60V, and my DRV8353RH has been damage very often at 50V~60V voltage range, it is quite stable at 20V~30V region. I am using the IRF7759L2PbF which is a Vds 75V MOSFET. According to Kim's experience using the MOSFET with higher Vds may have a possibility to solve the problem which I will be testing a couple days later, however I really want to know what might be the possible reason for this kind of fault to occur. To what we think is reasonable is that if there is a voltage overshoot then it suppose to be the MOSFET damaging, but what we observed is the DRV8353RH damage and the MOSFET is fine, when we substitute a DRV the controller still works. What we think is awkward is that the overshoot (77V~80V) we saw is still far behind the DRV8353RH absolute maximum (Vdrain).
I am persuading our manager team to let me move on changing the MOSFETs, but they can't accept that "if DRV8353RH is the one that fails, then why are we changing the MOSFET instead". Is there any mechanism inside DRV8353RH that cause this problem?
Best regards,
Jim Hsu .