Part Number: DRV10983
Other Parts Discussed in Thread: PCA9306
https://e2e.ti.com/support/interface/f/138/t/827817
"Can you help to explain more details of DRV10983 I2C port ?"
The 0.6V ViL is the INPUT low threshold which our device will be below. I do not see any VoL specs (the one we care about) in the datasheet for the DRV device.
If I don't want to use the internal 3V3 LDO,
Should I connect another 3V3 LDO 's output to the V3P3 pin,
Or leave the V3P3 pint unconnected ?