Other Parts Discussed in Thread: DRV8308
Hi Webmaster,
We are looking for a new motor driver.
Original, we are using DRV10974, but my customer's motor phase resistance is 0.7ohm.
Their motor designed for drone application.
And their system have to support 24000 rpm ~ 36000 rpm.
Do we have motor driver to support FG > 2000Hz?
I summarized their motor spec as below,
Operating voltage: 6V ~ 15V ( typical = 12V)
No load speed: 67200 rpm
Rated current: 0.8A max
Max current: 1.5A
Terminal resistance: 700mohm
Do you have any recommend 3phase motor driver?
Regards,
David