Hello
We are observing a weird issue on our last batch of board using a DRV8701. When the driver enter in brake mode to limit current, the GND seems very noisy and an ADC component on the board fails to acquire proper values.
Some boards works well some not at all.
We tried to measure the noise and some spikes about +/-2V appears on GND and VCC. However if we put the probe on a single pin one RSENSE terminals then all is OK. The DRV8701EVM board as a 1000pF between SP and SN which is not mentioned in the DRV8701 data sheet. Could it be related?
Our probe is a P2220 from Tektronix. If we change the attenuation from 1X to 10X then it fails again.
Probe characteristics seems to be
1X: 1MOhm 95pF in theory . (measured at 80 pF in practice)
10X: 10MOhm 16pF (measured at 18pF in practice)
There's no need for the probe to be connected to DSO, just GND and the probe so I assume this is something related with the RC characteristics of the probe.
Any tips to troubleshoots this issue?