Other Parts Discussed in Thread: MOTORWARE, DRV8301, LVBLDCMTR
Hello everyone,
I'm working on my graduate project, which is dual axis inertia inverted pendulum. I've tried to use sensorless systems i need to move my motor around 0 speed to get maximum torque, so i moved to sensored projects and added 2 quadrature encoders.
I've tried to run lab12b to run one motor with enco and it works good with both my motors, not indicating any problems. My goal was to use lab12c, but MotorWare projects tutorial says nothing about this one. I tried to run it but as soon as i set "Run_Identify" flag on any of my motors they just start to shake and draw a lot of current from my supply and heat up pretty fast. I've got speedref set default to 150RPM, increasing it just make current peak faster.
My main board is F28069M launchpad with two DRV8301 boosters. My motors are LVBLDCMTR model. My encoders have resolution of 500 impulses per revolution(that's the maximum i could get for my motors)
I'd be appreciated for any help.