Other Parts Discussed in Thread: DRV8301
Hi,
I recently checked out the datasheet and specs of the new DRV835x driver family. Since the part seems very sophisticated, we are currently planning to use the part in one of our customer's new designs. One thing that bothers me though, is the DRV835x's "Transient 200-ns high-side source sense pin voltage (SHx)" listed under absolute maximum ratings. The lower limit of -10V is actually really good compared to other half-bridge drivers, but the upper limit of VDRAIN + 10V limits phase voltage (VS) overshoot to 10V, if I understood this correctly. I have done lots of motor power electronics designs (also with TI drivers like DRV8301) and from my experience, keeping VS overshoot to less than 10V referenced to the dc-link voltage, is very stringent and hard to achieve when fast switching speeds are mandatory.
Does the DRV835x driver exhibit a higher VS overshoot tolerance if the overshoot duration is reduced to values significantly shorter than 200ns - let's say 10ns?
Does DRV8301 exhibit the same limitations concerning VS overshoot? The reason why I am asking this, is that we have been using this driver in lots of designs in the past years and until now there were no complaints of the parts failing, even if VS overshoot of 15-20V occurred (duration of overshoot: 5-10ns). Actually, according to our customer's feedback, the design is very robust.
Since we need to make a swift decision, if we will use DRV835x in the next design I am looking forward to a quick reply.
Thanks in advance.
Best regards,
Sebastian