Other Parts Discussed in Thread: TPS54040
Hi,
Can someone please throw in some light on the 2 questions that I am having ?
#1. There are 3 DRV8305 variants. (no LDO, 3.3V LDO and 5V LDO variant)
Does the PGOOD signal behave the same for the "no LDO" variant as with the 3V/5V LDO variant ?
(I was unable to find a satisfactory answer from the datasheet)
#2.
Both the TPS54040 and the DRV8305 both generate PGOOD signals.
Ref designs show the MCU is RESET using the PGOOD signal from the DRV8305.
Should the MCU be RESET from the PGOOD from the DRV8305, or from the TPS54040 ?
Thanks,
Manu