Team,
Customer was able to successfully identify and run a 24V, 4 pole pares motor with this EVM.
- In the lab they have a bigger motor, about 750W, 48V, 5 pole pares. This motor was identified when I decreased IQ full scale frequency to 400Hz but did not spin at all. Current never increased. What parameters and where can they alter to make the big motor spin?
- Customer brought the board back to his desk. Now it has a fault, GDUV Indicates VCP charge pump and/or VGLS undervoltage fault condition. Charge pump is dead. VCP voltage is only 1V above VDRAIN. He only applied 46V to the board. Why do you think caused this fault?
- Lastly, is this EVM able to be paired up with F28004x launchpad?
Thanks
Viktorija