This is a continuation of investigation about this issue:
https://e2e.ti.com/support/motor-drivers/f/38/t/837153
So I added an external 2Amp diode (Ifsm=150A) in parallel to the internal free wheeling diode from OUT to VM to have the high Inrush current flow through the external diode. The DRV8844 output still gets damaged. My initial theory that high inrush current that charges the bulk VM capacitors is not the problem here. I removed all external capacitors that are connected to VM and with or without the external diode, the DRV8844 output is still getting damaged.
I don't think that the outputs are protected for case like this, GND=0V, OUT=48V, VM=open. Can you please verify and let me know what is causing the damage?
We have a customer ready to order production samples but we can not move forward with this problem unresolved.
Thanks,