Part Number: DRV8837
Hi team,
Customer will use DRV8837 in the condition of VM=9V. They will connect a capacitor between OUTA and OUTB for reducing back EMF.
Could you check the maximum capacitance that can be connected between OUTA-OUTB?
I think there is a concern that the device can't turn on because OCP is asserted in the startup due to the inrush current if the capacitance is too large.
So, if you know how to decide the maximum capacitance between OUTA-OUTB, could you also explain it to me?
Regards,
Saito