Hi
some times our DRV8303 burns at power on or power off. The difference with previous PCB (which works fine) is slight, only place and route, the schematic and BOM are the same. What can I look at ?
best regards
Dominique Houzet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
some times our DRV8303 burns at power on or power off. The difference with previous PCB (which works fine) is slight, only place and route, the schematic and BOM are the same. What can I look at ?
best regards
Dominique Houzet
Dominique,
Thanks for posting on the MD forum!
Do you see any particular section of the device or it's pins getting damaged physically?
If you remove a damaged device from the PCB and compare it to a new unused device before it has been soldered to a PCB, can you tell me the differences in measurement from each pin to GND?
This would help us narrow down the issue.
Also please send a comparison of the two layout files.
Regards,
-Adam
we have a ref on the chip: 94AN06TG4
it burns several times just above the A, and near the right of the 4.
What value do I have to measure on the pins? Ohm?
How can I send you files (pcb)?
best regards
Dominique
Also, how do we use GATE_CURRENT field? I've first configured 1.7A, then 0.7, it seems that I've less burns with 0.7A!
Dominique,
Please send an image of the damage.
Sorry I forgot to mention that we want to see the resistance to GND in the above experiment.
This gate drive current sets the current driving the FET gates, I would start with lower settings and see if they work for your system without damage or excessive FET heating.
Which FETs are you using?
You can add me as a friend here and send the files privately.
Regards,
-Adam