Hello,
now my Motors work fine with my DRV8302 application, but the current measurement varies with the change of the operation voltage.
Example: with 24V Operation Voltage, the device switches off when current increases above 15A (Potentiometer adjust on OC_ADJ -Pin ) . With the same adjustment and 30V Operation voltage, the device switches of above 11A. The measured values on SO1 and SO2 are also wrong. . I double checked the correct wiring and refered to the design in DRV 8302 Datasheet. What can be wrong there?
Regards
Thilo