This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305: Ringing/oscillation on MOSFET gate.

Part Number: DRV8305

Hi Ti team,

We are using DRV8305 gate driver to finish a BLDC driver. We found really heavy oscillation on the MOSFET gate. we are using MOSFET: IPB042N10N3, no gate resistor, driving current set 100mA ON 200mA OFF, shown in below pictrue. You could see the negative spike is around -9.2V. I have questions below:

1. I only found this oscillation when bus current is big(like start up or with a heavy load), when the motor in free speed run(current around 3A), we did not see that. why? what caused the oscillation?

2. the Negative spike is -9.2V, duration is below 34ns, will it be a risk to damage the DRV?

3. Any suggestion to improve the oscillation? Add gs capacitor? 

Thanks!

Best regards,

Bruno Duan