Hello,
- Does DRV8889-Q1 have an automatic shoot-through prevention function in its each H-bridge? Or, does a dead time control have to be implemented in MCU in its control scheme?
- How will the DRV8889-Q1 behave when its output current doesn't reach its current regulation set point due to large load resistance, for example?
- Can the DRV8889-Q1 start with any phase when it's turned on?
- Does the DRV8889-Q1 require any sequence for external voltages including power supplies to be applied to its pins?
- I'm worried if some sequence would cause abnormal behavior or irregular current flow due to internal protection diodes, etc.
Best regards,
Shinichi Yokota