Hi team,
When DRV8847s works in parallel mode to control a BDC, which pin is used as input? Following table is only for DRV8847.
What's the true table of DRV8847s?
BR,
Naizeng
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
When DRV8847s works in parallel mode to control a BDC, which pin is used as input? Following table is only for DRV8847.
What's the true table of DRV8847s?
BR,
Naizeng
Hi Naizeng,
IN1 and IN2 control the outputs. IN3 and MODE must be set high to enable parallel mode.
Hi Naizeng,
Apologies.
IN1 and IN2 are still used to control the outputs.
Parallel Mode is set via the IC1_CON register in the DRV8847S.