Other Parts Discussed in Thread: CSD18541F5,
Hi,
we are using the DRV8323 to drive small MOSTETs type CSD18541F5 in 3x PWM mode to control a small 24V-BLDC motor (motor power 9W). See schematics below. If the PWM input is either low or high, current consumption of the circuit is okay (35mA including micro controller). But when toggling the PWM input, it seems that for a short period of time both high and low side MOSFET are on, as the current consumtion even with no motor connected (motor replaced by some LEDs to visualize the turning field) raises with the frequency of the PWM signal. We're using the default settings of the chip, except the Driver Control Register is set to 20h (PWM_MODE: 3x PWM enabled). The effect can be reduced by changing the dead time in OCP Control register from 100 to 400 ns, however there are still 300 mA flowing on 1 kHz PWM switching clock. The status doesn't show any error.
Do we need to change the configuration or is any addition external circuitry required with this small MOSFETs?
Thanks for any hint in advance
Karsten