Hi,
We are using the driver to control 2 mosfet half bridges. When the system is energized (not switching) the voltage in the middle point of the half bridge becomes 6.9V (SHA and SHB). We guess that voltage is coming from the driver, is that nominal beaviour? If that is a constant voltage provided by the driver, a large current will be drawn when a load is connected.