Hi,
I am considering using the DRC8876 CI in my new design and I am having problems with one of the failure modes that may occur to the circuit.
In my circuit the driver will battery-powered and will control a DC motor with direction control (probably in PH / EN mode). In one of the failure modes analyzed, there is a risk of the DC motor(6V 2A) being driven by the user (torque applied to the mechanism connected to it).In that condition the motor can operate as a generator and may induce a voltage at the driver output (OUT1, OUT2) in this scenario VM=0.
The driver can be damaged in this condition?
Any indication of protection for this failure mode?
I considered implementing "Reverse Supply Protection" in the VM input pin to prevent damage to the rest of my circuit. Would that be enough to protect the driver itself?
Note.: https://e2e.ti.com/support/motor-drivers/f/38/t/900354?tisearch=e2e-quicksearch&keymatch=reverse