Hello
My customer applied DRV10987 to the ceiling fan.
We request the setting value to operate with DRV10987.
Motor Codition is below
Voltage : 24V
Power : 40W
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
My customer applied DRV10987 to the ceiling fan.
We request the setting value to operate with DRV10987.
Motor Codition is below
Voltage : 24V
Power : 40W
Best Regards.
Hi Louis,
Thanks for posting your question in MD forum. We can provide recommendation for the EEPROM values that can be programmed based on the motor parameters and design parameters. Can you provide below information?
1. Phase to center tap resistance of the motor
2. Phase to center tap inductance of the motor
3. Back EMF constant Kt of the motor
4. Motor current rating
5. Number of pole pairs of the motor.
6. Rated mechanical speed of the motor.
Regards,
Vishnu
Hi Vishnu
I Provide the Motor Information.
1.Phase to center tap resistance of the motor
-> 0.92Ω (phase resistance) / 1.84 (line resistance)
2.Phase to center tap inductance of the motor
-> LS:6.0 / RS:4.34
3. Back EMF constant Kt of the motor
-> 14.4V (based on 360RPM)
4. Motor current rating
-> 16A
5. Number of pole pairs of the motor.
-> 18 Pole (STATOR) / 20 Pole (Magnet)
6. Rated mechanical speed of the motor
-> 360RPM
Best Regards.
Hi Louis,
Unfortunately we do not have any devices in DRV10x family that can meet your requirements. Max current rating in DRV10x devices is 3A. We have Gate driver ICs in DRV8x family with external control and FETs. Please let me know if you need more information on DRV8x devices so that I can redirect you to an expert.
Regards,
Vishnu
Hi Vishnu
Sorry, I Incorrect information was given.
Current Rating is 1.6A
Best Regards.
Hi Louis,
Thanks for the confirmation. DRV10987 will be able to drive your motor. Please refer to the DRV10987 Tuning Guide for tuning the device to your application.
Regards,
Vishnu
Hi Vishnu
I requested the setting value to operate with DRV10987.
and you said you could provide recommendations for EEPROM values.
I need recommendations EEPROM values for ceiling fan
Best regards.
You can use the below EEPROM values as a good starting point to tune your motor. Please note that these are just recommendations and you might have to do further tuning depending on the end application.
0x90 0x3C
0x91 0x5948
0x92 0x48
0x93 0x1C8A
0x94 0xA0
0x95 0x0
0x96 0x60
Regards,
Vishnu
Hi Vishnu
Thanks for your recommendations.
I will test with the recommended setting value.
Best regards.