Hi Team.
According to the following diagram, to avoid motor saturation, it is recommended that the Ifs current is less than the DC maximum current of the drive circuit. In this case, the corresponding current is the smallest when VM is minimum (in the case of vehicle battery voltage shortage). To ensure that the motor is not saturated in this case, Ifs The current should be set very small, but under normal voltage, because the motor driver chip is driven according to the Ifs current, its maximum output torque will be limited. If the phenomenon of motor saturation under low voltage is not considered, if Ifs is greater than the DC maximum circuit, then the How can the driver chip adjust the current when the motor saturation current cannot reach Ifs?