Hi,
I am getting an over current fault (reg 0x00, bit 11) during start up. It is Vcc dependent. If Vcc is 8V, the motor will run OK. If I increase above that, the motor will spin for a few seconds and stop, and keep retrying every 5 seconds. I need the motor to operate with a Vcc of 22V. I have the open loop current set to 0.4A and transition to closed loop operation disabled. I don't have a current probe for my scope, so I don't know what the actual current is. I can only measure the current in the ground leg to the power supply using a 0.1 ohm resistor. That current peaks at about 0.5A.
I am wondering if the motor winding has too little inductance. Are there ever situations when you need to add fixed inductors in series with each motor phase?
Thanks,
Dave Gustavson