We are having two issues with our implementation of the DRV8711.
First we are seeing somewhat frequent damage to the gate drivers of the DRV8711, it seems more frequently the low side drivers are experiencing damage. The damage is measured by measuring the gate driver impedance to ground. Typical/unused DRV8711 low side gate drivers have an impedance of ~150kOhms to ground, high side around 500kOhms. What could be causing this damage to the DRV8711? We don't measure any violation of the absolute maximums of the part so far on the gate drivers. Is there anything we should review or measure that might lead us to the source of the damage? The FETs appear to be unaffected/undamaged in this scenario.
We also are experiencing driver damage and FET damage but we are extremely confused because:"
- we don't have a load attached to the power stage
- The DRV8711 doesn't appear to ever get enabled via SPI (CS is always low)
- The DRV8711 is held in RESET via the RESET pin relatively soon after power up (SLEEPn is always pulled high)
What could be causing such failures and damage to both the FETs and DRV?
Could transients on the AOUTx/BOUTx or ISENSEx pins cause damage to the gate drivers, particularly the low side drivers?
Here is the schematic: