Hi Team,
I want to control a capacitive load with the DRV2667.
Is it possible to create non-symmetric signals like sawtooth or rectangle profiles?
The DRV2667 has two options to create the output signals. PWM input signal or Waveform Synthesizer.
The PWM seems to be more appropriate. But the problem I still see is that the two output channels cannot be controlled independently. That means I cannot create a sawtooth signal with changing halfwaves like in the attached schema (positive, negative positive,...). Is that right?
Beat Regards,
Tom Liu