This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8302: Maximum current and watt

Part Number: DRV8302
Other Parts Discussed in Thread: DRV8301, DRV832X, , UCC27710, UCC27712, UCC27712-Q1

Hi;

rozum.com/.../controller-rozum-robotics.jpg

I want to ask for the link above. 8302 was used here. The power of the motors is at least 225Watt (for 48V). Is it possible to use these motors at full power with 8302 with 1.7A current?

Or are the values given on peak?