Dear Yanming:
My clients refer to the board designed by boost xl-drv8301 to sample three-phase output voltage and output current. The current sampling is the lower bridge arm resistance sampling of three-phase current. The current sampling resistance is 20mohm, and the current sampling amplifier is 8.45 times. The software is based on proj_ lab13b.
It adopts 48V PMSM motor; the rated current is 8.2A; the rated speed is 3000rpm; the rated torque is 1.27nm; the pole pairs are 4;
The positive and negative rotation of the motor is OK. Here are some of my hardware and software settings:
USER_IQ_FULL_SCALE_VOLTAGE_V (48.0) USER_IQ_FULL_SCALE_CURRENT_A (21.0) USER_ADC_FULL_SCALE_CURRENT_A (39.0) #define USER_NUM_CURRENT_SENSORS (3)
The parameters of the motor are set as follows:
USER_MOTOR_MAX_CURRENT (11.6) // 8.2*1.414= 11.6A; USER_MOTOR_VOLT_MAX (48.0)
Questions are below:
When the motor is under partial load, at a certain speed, such as about 1800rpm, it can be seen through CCS debugging window that Id_ref has reached 9.8A and motor torque has reached 0.73nm; but at this time, the ammeter connected in series in the DC bus circuit shows that the actual current is only 3.5A.
Why is the difference between control current and actual current so great?
Best regards