This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 37
Part Number: DRV8886
Hello team!
I got 2 questions from the customer. Would you mind supporting those, please?
1: For regulation current accuracy, what's tolerant on TRQ value? Is this exactly 50 or 75 or 100%?
I'm assuming that the RREF & ARREF values are more dominant for the accuracy but just want to confirm the TRQ% affect it or not.
2: It is allowed to input signals in the logic pin before implying 24V in VM, correct?
Aside from the DECAY pin, there's an internal pull-down register for all logic pin so I think this should be fine.
Thank you for your support.
Best Regards,
Kazuki Kitajima
Kitajima-san,
1. You can treat 50 or 75 or 100% TRQ value is an exactly number without error.
2. "It is allowed to input signals in the logic pin before implying 24V in VM" The IC would be safe if the input signal voltage is below the maximum voltage rating spec.
Wang Li
Motor Drive Solutions
In reply to Wang5577:
Wang-san,
Thanks!
I understood.