Other Parts Discussed in Thread: DRV10987EVM
Drv10983 Over current protection.
Hi,
I am driving Maxon motor using Drv10983 via I2C interface. I am able to configure the EEPROM registers and read back the data.
Without connecting the motor the driver gives the over current status, which from data sheet defines that phase to phase connection is shorted.
If speed is enabled via PWM of 5% duty cycle, i can see the over current and motor lock status read from driver.
How can i over come this problem. Please suggest.