This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 68
Part Number: DRV8837
Hello,
Is it required to connect a varistor or birectional TVS diode in parallel to motor for protection against high voltage spikes? or does the IC provides protection against inductor current?
Hi Jain,
The DRV8837 includes over-current protection. If the output current is above 1.9A for longer than the deglitch time of 1µs, the H-bridge FETs will be disabled protecting both the driver and the motor. If you wish to further protect against sudden voltage spikes, you can add a varistor or TVS diode.
Regards,Pablo ArmetMotor Applications Team