Hi, I'm evaluating specification of daisy chain enabled motor driver for current project.
Our requirement is to run 20 * 22 module matrix of small 12V at 15Hz refresh rate.
We are planning to have the driver on each module just for plug and play installation and handling purpose.
It will be distributed in 4000 * 5300 mm space, so single daisy chain would easily get up to 100m in total length.
(Vmm will be supplied at multiple points in parallel, Vdd supplied separately with LDO from Vmm)
Our concern is the length of the chain and its bandwidth speed.
- Does the driver repeat the shifted out data or just passthrough them?
- (200ns * 16bit) * (20 * 22) is about 710Hz, is this correct way of calculating refresh rate?
- what happens to the chain if single module fails in the middle?
Is it feasible solution?
I'm open to any other recommendation or solutions
Thank you in advance.