This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8885: OUTPUT CURRENT

Part Number: DRV8885

Hello,

When the motor driver was set to 1/8 with indexer,
it was written that AOUT CURRENT was 71% of full-scale and BOUT CURRENT was 71% of full-scale by default.
Does it mean that if the user uses the TRQ pin, it can be further 75% or even 50% from here? (Full scale x 71%)x75% or (Full scale x 71%)x50%

Best regards,
DDdoor