Dear Sir,
We use your motor driver IC DRV8662.
It fails so often. We estimate some causes for the failures.
Would you pleae tell me your advices?
1) We ues that IC in 200V output mode. We apply 200 to 300 Hz rectagle waveform.
During our operation, the Enable input is set to High. We measured the current. The magnitude of current was 0.18 A.
According to the datasheet, at 300Hz in 200V mode, the consumption current is 400 mA. We regard 0.18 A is within the tolerance,
and think our operation is allowable.
My idea is corrent?
2)The ouput teminals are connected to a tiny connector. The receptacles which connet each IC output are ajacent. Due to position tolerance of the plug and receptacle,
we suspect ajacent terminals may be short circuited. If that happen, does that IC fail? Or over current can be detected by the thermal sensor and the sensor will switch off
the ciruit?
I think if that IC have some protection circuit at the output terminal, the IC will not fail so easily. Does that IC have that kind of protection circuit?
Regards,
Shozo Ohtera