Other Parts Discussed in Thread: DRV8323
Hi,
we have designed a motor controller based on the eval. board BOOSTXL-DRV8323RS(DRV8323RHRGZR)
Our board never releases nFault.
We have compared all the readings of our board to the eval. board and they are all similar.
Voltage 12V and 18mA
Have tried with 24V with the same result.
nFault pin. It resets every 4ms when INHA, INHB, INHC is set to low by the MCU.
Nfault with 15kHz PWM signal
MOT_A with PWM signal:
MOT_B with PWM signal
MOT_C with PWM signal