This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8305EVM: Parallel Configuration for Higher Output Current

Part Number: BOOSTXL-DRV8305EVM
Other Parts Discussed in Thread: DRV8305, DRV8320, DRV832X

Hi Team,

Posting on behalf of our customer. Can they use two DRV8305 booster packs (BOOSTXL-DRV8305EVM) in parallel to drive a high current motor? The EVM can deliver up to 20A but they need to drive a 35A motor. If this is applicable what are the critical parameters/conditions that needs to be considered?


Kind Regards,

Jejomar