Hi,
I have a question related to the register configuration of DRV8889-Q1.
I am following the steps to configure the registers on this device , I have a question about this sequence.
1. Driver on - DRVOFF - LOW
2. Sleep mode off- nSLEEP - HIGH
3. Configure micro-stepping mode - CTRL 3 register (using SPI write)
4. Configure open load detection enable - CTRL 4 register ( using SPI write)
5. Configure stall detection - CTRL 5 register (using SPI write)
What happens if I write the nSLEEP to low and in a delay of 1 ms write it to high?
Something like this:
GPIO_write(nSLEEP_INDEX, LOW); Osal_delay(1); // 1 ms delay GPIO_write(nSLEEP_INDEX, HIGH);
Will I lose my register configurations?
Thank you,
Arshiya Tabassum
What happens if I