Hi team,
I would like to get your input with the customer inquiry below:
In the customer design, With Rsense=100 mohms, , he has a max of 1.2A chopping current with the driver OUT1/2 (voltages) being chopped when supplied with a VM=24V. But if he reduce the Rsense to 50mohms, they see a constant current of 1.2A with VM=24V, no voltage drops noticed at OUT1/2 pins. But if calculate Ichop max, as per the datasheet with Vref=3.3V and Rsense=50mohm, they get a Ichop of 13.2A max : which is confusing. So they question is what is the min current sense resistor I can use, and what is the advantage/disadvantage going with a real low value( of Rsense like 25mohms )?
I will send the schematic via email if you want to check it.
Thanks,
Jonathan