This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8838: Data Transfer using isolator transformer

Part Number: DRV8838
Other Parts Discussed in Thread: DRV8837

Hello

Can I use DRV8838 or DRV8837 for transmitting digital data in low frequency like 2400bps using isolator transformer ?

I need to change the polarity of the primary winding repetitively.

some ICs like ZXBM5210 recommends to keep direction change frequency of below 400Hz.

Is there any limitation for repetitive direction changes ?

( ZXBM5210 Datasheet - page 6  --> If repetitive direction changes required, it is recommended to keep direction change frequency of below 400Hz)

Thanks.