Part Number: DRV10987
Hi Team,
The customer is experiencing below issue and needs your help.
The FG signal of drv10987 is the real-time feedback motor speed signal of stable closed-loop state, When error is detected ,the FG signal will be pulled up to "High". But now a problem is found in the application, when the U\V\W are in poor contact or no contact(Before the no contact the motor works normally), FG outputs PWM signal and the frequency decreases gradually ( config detect no Motor Fault), In this way, the system mistakenly assumes that the motor is still rotating. So how to set the config register to feedback the condition of no contact of U\V\W?
Now my EEPROM Config is follow:
0X90 0X102E
0X91 0X0B3A
0X92 0X08C0
0X93 0X12EB
0X94 0X3B0F
0X95 0XF843
0X96 0X006A
Thanks,
Annie