Hi Team,
I have a couple of questions from the customer regarding DRV8889-Q1 below:
The customer is looking at using a motor with Rcoil=5.6 ohm, and current rating of .67A. This leaves rated voltage of 3.8 volts. He will have a Vm of around 22V (adjustable if lower voltage is desired).
Here are the questions:
One is, "Will the DRV8889 (assuming Vref and TRQ_DAQ set appropriately) be able to regulate to 0.67 A, where the voltage across the coils are 3.8V (steady state)?". If the answer to the first question is yes, then how low can the current be adjusted in a steady state. i.e. to hold the motor in a fixed location, can the driver still regulate the current down to say .3A which would be a voltage of 1.68 V across the coils? How low can the driver work in steady state in terms of voltage across the coils?
Thanks,
Jonathan