Part Number: DRV10975
Hi,
If I have system with input voltage (VCC) is 12V, if the VCC voltage is cut, will the AVS function still work? When does the IC cut off this functionality?
On the programming, how does the different modes affects the register programming :
1. If I exit standby mode, do I need to re-program the driver IC parameters?
2. If I use the DRV10975 variant which has the sleep mode, do I need to re-program the driver IC parameters when I exit sleep mode?
Thanks,
Christina