Hi team, trying to run 3.3 V stepper motor with the DRV8889 and getting UVLO fault. Powering it with a 9V battery and am reading ~8V at Vm, which is well above the 4.5V min.
Do you have a similar encounter?
Thank you very much.
-Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team, trying to run 3.3 V stepper motor with the DRV8889 and getting UVLO fault. Powering it with a 9V battery and am reading ~8V at Vm, which is well above the 4.5V min.
Do you have a similar encounter?
Thank you very much.
-Mark
Mark,
Can you please give me some more details on your setup? Is it your own design or an EVM from TI?
If own design, can you please share schematic.
Have you checked with an oscilloscope to see if the supply is dropping below 8V under load?
Hi Ryan, my customer is using TI Board for this application. I am waiting for their measurements.
Thank you for supporting this post.
Mark,
OK. When responding, please also provide the revision of the board...should be a MDxxxxx label on it. If you can give me that label information, it would help me make sure it is the latest EVM. Also, revision of GUI they are using would also be helpful.