I am trying to build an art piece in which I can spin it in a controlled fashion. I need to be able to go forwards and backwards. There are two pieces of art. One is bigger and the other is smaller. They will be spinning at the same time. The bigger one is about 10lbs or so and the other is about 3-4lbs. I need to spin them both in different directions. I need to know how fast they are spinning. I'd love to control all this through my laptop. So I guess I'd need the software as well. :)
So I have no idea where to begin as far as motor size, bipolar or unipolar? What type of controller would work in this application. I'm assuming this is a fairly simple project but I've never done anything like this. I'm really good at building things and figuring things out, but at this time I'd love to get a little ahead so I can do it fairly soon. Also, I don't have a lot of money so that would be yet another factor. And if anyone here has parts that would work in this application, that would be willing to sell to me.
Thanks!
Steve