Hello,
I am looking DRV8332-HT datasheet and I don't understand thermal shutdown part :
Overtemperature Protection
The DRV8332 has a two-level temperature-protection
system that asserts an active-low warning signal
OTW) when the device junction temperature exceeds 125°C (nominal) and, if the device junction
temperature exceeds 150°C (nominal), the device is
put into thermal shutdown, resulting in all half-bridge
outputs being set in the high-impedance (Hi-Z) state
and FAULT being asserted low. OTSD is latched in
this case and RESET_A, RESET_B, and RESET_C
must be asserted low to clear the latch.
So the maximum operating junction temperature is 150 deg ?
The thermal shutdown is the same than non HT version ?
Best regards
Maël Guilbaud