Other Parts Discussed in Thread: DRV8813, DRV8818, DRV8811
Hi,
I got some question about DRV8813 behavior,
1. My customer tested two different stepping motor with DRV8813 as following settings,
VM=12V , Decay=Low(slow) Vref=0.32V , RISENSE=0.47Ω (so, Ichop=0.32/(5*0.47)=0.136A)
As a result, on of them seemed to work correctly (Ichop=0.134A)
but the Ichop of the another motor exceeded the setting value (Ichop=0.257A)
and when the Decay set to High(fast), both of them seemed to work correctly (Ichop was about 0.12A)
What is the possible cause of this behavior?
2. Regarding the attached waveform,
Is the Aout1 output voltage waveform correct?
Why does the Aout1 output current increase when Aout1 output voltage is low?
3. what is the advantage and disadvantage of these two Decay mode (fast and slow)?
Thanks
Go