Other Parts Discussed in Thread: DRV8818
Hi
My customer is using DRV8818.
He requests the following information of Thermal shutdown function.
Please advice me.
1. Why is the thermal shutdown temperature larger than the absolute maximum operating junction temperature value(Min:150, Typ:160, Max 170)?
-> I think that it is because the method of realizing the thermal shutdown function has an error.
so, minimum value is 150 degree.
2. How to return normal mode after thermal shutdown operating?
->Does it return automatically by being under 150 degree?
or the reset of DRV is needed?
Best regards
Shimizu.