Hi,
Can I drive a latching relay coil with 2 inverted outputs of ULN2003V12PWR?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I drive a latching relay coil with 2 inverted outputs of ULN2003V12PWR?
Hi,
ULN2003V12PWR may not have the ability to reverse the direction of voltage. But I can connect the end of relay coil to OUT1 and OUT2 and make only one of the OUTs high and the other low. A similar circuit is given in Figure 7 of datasheet (
).
Won't the above combination work for a latching relay coil?
Hi,
Please refer to the below link:
http://m.eet.com/media/1126690/11142-figure_1.pdf
I want to build a similar circuit with ULN2003V12PWR without 47 ohm and 4.7 ohm resistors in the above circuit (and directly connect OUT1 and OUT2 to relay coil).
Please advise.
Regards
Srikanth